Part Number: LMX2594 Hi all,
Can we replace the muxout pin with the read back of R110[10:9] for the LD of lmx2594?
And what's the difference between muxout LD and R110 LD of lmx2594?
Regards
Part Number: LMX2594 If using the LMX2594 to generate 11-12G and 12-13G frequency-sweep signals under a 10M input signal condition, with a signal bandwidth of approximately 1G and a sweep time ranging from 0.1 to 3ms, it is important to pay attention…
Part Number: LMX2594 Hello,
The customer has been able to achieve phase synchronization of multiple LMX2594 chips. However, a new anomaly has occurred during use. When monitoring the output of four clocks using an oscilloscope, there is a probability…
Part Number: LMX2594 Hi, I'm currently using LMX2594 to generate a signal between 7-10GHz, and is used as an LO signal for the mixer. During the siimulation of PLLatinuum, I found that there always exists a peak at about 1e5 phase noise when I'm designing…
Part Number: LMX2594 Regarding Pout, I would like to know the voltage level instead of dBm. Is the following conversion formula correct? Especially, whether dBm should be converted using 10log or 20log often varies depending on the manufacturer, so I…
Part Number: LMX2594 Hello!
Differential RF output frequency is 915MHz, the RF output RFoutAM/RFoutAP are pulluped 50R connected to VccRF.
Can we configure LMX2594 differential RF 915MHz output power is 10dBm?If it is true, how to set the related…
Part Number: LMX2594 Hi Ti pll experts,
There are 4 lmx2594 synthesizers in my design to generate the same outputs locked to the same input reference, and the input references are from the digital phase-locked loop.The block diagram as bellow,
Now…
Part Number: LMX2594 Regarding the LMX2594 registers, I'd like to know:
1. Is there an officially recommended time order for register configuration? For example, power on first, then set the frequency and power, then lock, then read back. Is there a…
Part Number: LMX2594 Dear TI Signal Chain Support Team,
I am currently working on a high-performance clocking design using the LMX2594 . I have a specific question regarding the phase determinism of RFoutA when the chip is operating in SYSREF Master…