Part Number: LMX2595 I have a few questions regarding the LMX2595 and its ramping capabilities:
VCO Architecture Could you please clarify whether the LMX2595 uses a single VCO or multiple VCOs internally?
Best Method for Frequency Sweeping I would…
Part Number: LMX2595
Dear TI Technical Support Team,
I am currently working with the LMX2595 and I would like to use a BALUN to combine the differential outputs RFoutAP and RFoutAM into a single-ended output.
I have the following questions:
1…
Part Number: LMX2595 Other Parts Discussed in Thread: LMX2491 Hello,
Can we use LMX2595 to produce a cw sawtooth wave that as an LO for mixer. The range of frequncy is 75MHz, the period is 25 us, as the figure show:
How can we configure the chip…
Part Number: LMX2595 Hi there,
I have a question about the sync with multi LMX2595s.
Doing the sync @10GHz(OSCin: 125MHz), I change Charge Pump and Delay in oder to synchronize the phase.
Every LMX2595s have their own Charge Pump and Delay value…
Part Number: LMX2595 I'm looking at the LMX2595 datasheet, SNAS736C – June 2017 – Revised April 2019.
Question 1:
I've read the explanation in "7.3.11.1 General Concepts" in the datasheet, and I understand that
t1 and t2 indicate the time when synchronization…
Part Number: LMX2595 Other Parts Discussed in Thread: LMX2594 Could you suggest synthesizers that works using 10MHz as reference and generates 12.8GHz with below mentioned phase noise specs.
Offset
Phase noise
100Hz
-60dBc/Hz
1KHz…
Part Number: LMX2595 Hello,
We are using LMX2595 to generate 12.8GHz from a 70MHz reference. Internal doubler is enabled and the charge pump current is 15mA. It is found that the LMX2595 is generating spurious frequencies at +/- 140MHz away from 12…
Part Number: LMX2595 Tool/software:
Hi,TI team:
During mass production, one LMX2595 card experienced an abnormal lockup.
Measurements revealed that the CPOUT pin voltage was approximately 2.5V when powered on and unconfigured (a normal voltage for…
Part Number: LMX2595 Tool/software: hello
i use the lmx2595 with partial assist
i have problem to lock the device
oncy second command lock the pll
delay below 3 mSec between first and second round dont lock the pll
delay of 3 mSEc the pll…