Part Number: LMX2615-SP Other Parts Discussed in Thread: LMX2624-SP lmx2615-sp_DEC 2025.pdf lmx2615-sp_MAY 2020.pdf
Is the specification of output of lmx2615-sp really changed?
PLL_bufferAMP_output.pptx
Part Number: LMX2615-SP Hello,
I would like to share the SPI bus for two LMX2615-SP parts with Serial Data Output for readback on the MUXOUT pin. Although the datasheet suggests this is possible by setting MUXOUT_CTRL=0 the default setting for this…
Part Number: LMX2615-SP Other Parts Discussed in Thread: AFE7950-SP , , LMK04832-SP , LMK04832 , AFE7950 Hi,
We are using LMX2615-SP part in one of our custom boards. I am deriving 2 output clocks from LMX device, one used as the device clock for AFE7950…
Part Number: LMX2615-SP HI Team,
I am looking for information regarding input drive (dBm) vs expected phase noise performance for the LMX2615-SP.
That is to say, will the phase noise performance of the LMX2615-SP change drastically over input…
Hi Deepak,
It looks like the device is cycling between lock and unlock states. To troubleshoot this further, please provide the following information:
The output swing of the 10MHz sine wave at the LMX2615-SP OSCin pin.
Whether this issue is isolated…
Part Number: LMX2615-SP Hello,
We are currently using the LMX2615 to generate 65.472 MHz from a 10.23 MHz reference.
At room temperature (25°C), the PLL locks and operates normally. However, at low temperature (-25°C), we are seeing an unlock issue…
Hi again Szymon,
I did a bit more digging and found a few more resources:
LMX2615-SP: Lead Forming Specification for the LMX2615-SPLMX2615-SP: Assembly application note or guidelines
Thanks,
Michael
Part Number: LMX2615-SP Tool/software: I want to generate 65.472 when the reference clock is 10.23 MHz.
I made the output clock using the TICS Pro.
However, it does not work.
I attach the file. Could you review the file or send the load file of…
Part Number: LMX2615-SP I'm supplying the VccVCO (pin 57) and VccVCO2 (pin 41) through a ferrite bead, and want to understand the expected current draw of these pins during nominal operation. I see that the total Vcc current is typically 360 mA. How much…
Part Number: LMX2615-SP Other Parts Discussed in Thread: LMK04832 Hi Experts,
I'm using a single LMX2615 in a design, and had a question regarding VCO_PHASE_SYNC. In my application, the part takes in a 100 MHz reference, uses the x2 input frequency…