Part Number: LMX2615-SP Tool/software: Does this termination scheme work for these 2 parts. We don't trust the LMX IBIS model. The ADC is ADC12DJ5200.
Thanks,
Part Number: LMX2615-SP Tool/software: Dear Team,
1. The data sheet recommends to connect 10 uf capacitor at pin 7,25, 41, 44,53, 56 and 57.
Please comment if a lower value of capacitance can be connected.
2. Can a combination of capacitance be…
Part Number: LMX2615-SP Tool/software: The Datasheet mentions to terminate an unused RF output but also shows that you can shut down the unused output via SPI control which would seem to make the termination irrelevant. We plan to shut down the unused…
Hi Yevgeniy, Please note LVDS works. Refer to this past thread: https://e2e.ti.com/support/clock-timing-group/clock-and-timing/f/clock-timing-forum/1081675/lmx2615-sp-lvds-driver?tisearch=e2e-sitesearch&keymatch=LMX2615-SP
e2e.ti.com/.../lmx2615-sp…
Part Number: LMX2615-SP Other Parts Discussed in Thread: LMX2594EVM Tool/software: Hello
Now I am testing LMX2615-SP.
I use TICS Pro to obtain Register MAP.
For the datasheet, the division value is equivalent to 72.
However, there is no value…
Part Number: LMX2615-SP Tool/software: Hi,
We are utilizing a resistor pullup configuration for our LMX that is outputting a 2.5Ghz clock. We currently have the OUTx_PWR set to 63. The resistors we have on the output are 50ohm,1206 size, 250mW resistors…
Part Number: LMX2615-SP Tool/software: Part-1 (capacitance connection)
Can a common 10 uF capacitance be used for pins 25,41 and 57 (VCC Mash, VCCVCO2 and VCCVCO respectively),
or should they be individually terminated using 10uF capacitance each…
Part Number: LMX2615-SP Tool/software: Hi,
I am using the LMX2615-sp to change frequencies at ~100 Hz as part of a PID controller.
I have noticed that changing PLL frequencies using the calibration sequence (FCAL_EN = 1) causes large, undesirable…
Part Number: LMX2615-SP Tool/software: Hi,
I am using LMX2615 for clocking the RF DAC.So I am configuring LMX2615 in the "TICS pro"
In TICS Pro,I need to give 187.5MHz as FOSC and need to generate 12GHz from RFOutA and also need to generate SYSREF…
Part Number: LMX2615-SP Other Parts Discussed in Thread: LMK04832 , LMK04832-SP Tool/software: My customer is planning on using the LMX2615-SP to clock high speed data converters on a space project. He needs to clock the ADC at 11.520 GHz and here is…