Part Number: LMX2694-EP Other Parts Discussed in Thread: LMX2820 Where can I obtain an IBIS model for the digital interfaces (SPI, Muxout, En) of LMX2694-EP ? Is there a similar part's IBIS we could use, if there is not an IBIS model for this part? T…
Part Number: LMX2694-EP Hello,
As LMX2694-EP is pogrammed through SPI, the control board we plan to use to program LMX2694-EP can provide maximum 500Hz SCLK.
I would like to ask if is there minimum and maximum SCLK frequencies for LMX2694-EP SPI interface…
Part Number: LMX2694-EP Other Parts Discussed in Thread: CDCLVP111 , ADS5474 , LMK04368-EP , LMK04832-SP , LMK04832-SEP Hi,
LMX2694 and CDCLVP111 will be used for clocking for 4 ADC.
The LMX2694 supposed to provide 54-fs RMS jitter and CDCLVP111 buffer…
Part Number: LMX2694-EP
hi all,
The output frequency of my product is 11.3625GHz, which is 1.6GHz away from the main frequency and 1.4GHz has spurt. Why is it there? Can we eliminate it?
The reference clock frequency is 100MHz.
Phase detection…
Part Number: LMX2694-EP Other Parts Discussed in Thread: AFE7953 , LMX2594 Dear TI E2E Community,
We need to use AFE7953 Sync mode with FPGA with keeping JESD clock generated from LMX2694, As AFE has differential output for Sync and LMX support only…
Part Number: LMX2694-EP Hello,
Referring to the LMX2694-EP datasheet, the two orderable part numbers below are the same product.
What does the V62/19616-01XE part number mean?
When should LMX2694-EP users use this part number?
Thank you.
…
Part Number: LMX2694-EP Other Parts Discussed in Thread: PLLATINUMSIM-SW Hi Team,
Using the LMX2694-EP chip to output signals, spurs were found on the near end of some of the band signals when testing the output of the 500-6000M band. For example, at…
Part Number: LMX2694-EP Other Parts Discussed in Thread: LMX2594 Hello,
On the datasheet, it is written that the performance is measured using a clean 100-MHz input reference but no additional information is provided about how clean it is.
I know…
Part Number: LMX2694-EP We will not be using RFOUTB and will configure R44 to power down this output. Figure 8-7 (Termination of Unused Output - Differential) in the datasheet shows to use 11 parts to terminate an unused output... 11 parts! Is this correct…
Part Number: LMX2694-EP Hi,
when I create a register set for the LMX2694 using the TI TICS tool I get different values for the reserved registes that when I follow the datasheet.
Here are a few Examples:
Reg 4: Datasheet 0xA43 / TICS 0xE43
Reg…