Part Number: LMX2820 Tool/software: The peripheral strictly follows the circuit and parameters of the lmx2820 demo board. The FPGA used for control has successfully sent and read back register data, proving that the data has been successfully configured…
Part Number: LMX2820 Tool/software: Hi all,
The datasheet for the LMX2820 lists the max VOSCin differential input voltage as 1Vpp.
Is this the total differential swing allowed between pins?
There's a note "(6) See applications section for definition…
Part Number: LMX2820 Tool/software: Hi,
According to the schematic of LMX2820, CPOUT and VTUNE require three capacitors: 68nF, 2.2nF, and 480pF. However, we currently lack the 68nF and 2.2nF capacitors. Can we use capacitors with other values as substitutes…
Part Number: LMX2820 Tool/software: HI!
After the LMX2820 instant calibration initialization, the frequency was changed from 5.65GHz to 10GHz. The LD lock time is 6 seconds. Procedure Without power off, 10GHz lock off after even calibration: R1:0X57A0…
Part Number: LMX2820 Other Parts Discussed in Thread: LMX1204 , Tool/software: Dear Specialists,
My customer is evaluating LMX2820 and LMX1204.
They have a question about SYSREF of LMX2820.
I would be grateful if you could advise.
---
We have…
Part Number: LMX2820 Tool/software: Dear Team, I am using the LMX2820 PLL in my application to generate Ku-band single-tone signal. A clean and stable 100 MHz reference from TCXO is provided to the device. However, I am observing in-band spurious signals…
Part Number: LMX2820 Tool/software: Hi Team,
I'm using the LMX2820 PLL IC on my board and interfacing it with USB to Any. I’ve connected a 10-pin ribbon cable on one side (to USB to Any) and a micro-D connector on the other. While the device is detected…
Part Number: LMX2820 Tool/software: Hi,
I have some problems in phase synchronize multiple LMX2820 devices.I use an external sync signal to synchronize two LMX2820 chips after setting a frequency for each chip. But it seems that synchronization fails…
Part Number: LMX2820 Tool/software: Hi,
As shown in the topology below, the LMX2820 works in Cat.3 synchronization mode. Whether to support the phase alignment of the output clocks of two chips, the error phase between the two outputs is fixed.
There…
Part Number: LMX2820 Tool/software: Hi team,
My customer use the LMX2820 and find the MUXOUT pin don't have output. If you have any suggestions of the software configuration to solve the SPI communication? Thanks.