Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: LP38693
[Case:612982]Technical Data Inquiry for our customer.
SiliconExpert is contracted by our customer to work with their suppliers for accuracy and compliance purposes.
Could you please provide us with the reactivation reason as the part…
Other Parts Discussed in Thread: LP38693-ADJ Hi There,
I am looking at using the LP38693-ADJ - 500mA Low Dropout CMOS Linear Regulators with Adjustable Output Stable with Enable pin. The datasheet states the quiescent current during shutdown (EN < 0.4…
Other Parts Discussed in Thread: TPS7A26 , TLV767 , LP38693-ADJ , LP38691-ADJ Hi Team,
There is a good news that we have a chance to replace "NCP3335AMN330R2G"
Do we have a solution to replace "NCP3335AMN330R2G" ?
The URL below is "NCP3335AMN330R2G…
Part Number: LP38691-ADJ Other Parts Discussed in Thread: LP38691 , LP38693 Hi Team,
A quick question here:
Currently looking to use the LP3869x-ADJ as our ldo for one of our products. One thing I noticed is that the LP38691 does not have a enable pin and…
Part Number: TPS7A16 Other Parts Discussed in Thread: LP38693-ADJ Hello Team,
can TPS7A1601 be used as a current source for 5...10mA and a voltage of 50V similar to the LED schematics shown in TIDU922A ?
Can you provide the schematics for such an application…
Part Number: LP38692-ADJ Other Parts Discussed in Thread: LP38693-ADJEV Hi Team
. Could you send me Gerbers and schematic for AN-1757 LP38693SD-ADJ Evaluation Board please, because they are missing from your webpage?
Hi Steen,
With the part number that you listed, I believe you may be referring to the incorrect datasheet. Please be sure to use the LP38693-ADJ datasheet .
The primary source of inaccuracy with a linear regulator is the internal reference. Please refer…
Part Number: INA195 Other Parts Discussed in Thread: TLV3201 , LM27761 , LMP8646 , LP38693-ADJ , LP38693 I want to limit o/p current limit at 10mA for -3.5V supply regulator.
Can we use current sense INA195 and comparator TLV3201 to control the EN pin of…
Part Number: LP38693 Hi,
If possible we would like to know the output voltage tollerences for LP38693SDX-ADJ/NOPB in the following conditions:
Vin: 5.0V, Vout 1.8V, Iout 20mA, Temp range 0-55degC
Other Parts Discussed in Thread: LP38693 , LP38692-ADJ Hi There,
We have a battery powered application that consumes typically a few tens of uA in its low power mode.
The system uses two LP38693 regulators: -
LP38693SD-3.3
LP38693SD-5.0
When the system…