Other Parts Discussed in Thread: LM339-N , LM339 , LMC7215 , TLV3691 , LPV7215 , TLV3701 , TLV3401 , LP339 , TLC339 , TLC3704 , REF3325 , REF1112 The Output sink current of LM339-N is specified as 6mA min.
Since this part has an open collector output, does it mean…
Denis,
There is the TLV3501 in 6 lead SOT-23. Vin max 0.2V from V+.
Did you need it in 6 lead SOT-23 for the shutdown function? If you don't need shutdown and 5 lead SOT-23 works we also have from highest Vin max to lowest:
LPV7215, LMV7239, LMC7211…
Other Parts Discussed in Thread: OPA379 , LPV7215 I am using OPA379 Single supply ultra low power opamp for SIne to Square wave converter...(ZERO CROSSING DETECTOR)
Input is 20mV pk-pk AC Sine wave from Current Transformer..
Supply voltage is 3.6V battery…
Other Parts Discussed in Thread: LM139 , LM139-N , LM339 , LMC7211 , LPV7215 , LMC7221 I got the below question:
Problem: I would like to use comparator LM139 or similar normal operation: single supply 15V input - 14.5V input + 10v output : open collector unnormal…