Part Number: LSF0108-Q1 Other Parts Discussed in Thread: TXU0104-Q1 , , TXU0204-Q1 , TXU0304-Q1 Tool/software: ■Q uestion
① Does this model support I2S interface? ※I would like to confirm this as it is not mentioned in the datasheet.
② Can this…
Part Number: LSF0108-Q1 Tool/software: Hello,
I'm evaluating the use of the LSF0108-Q1 level shifter for a 160 MHz QSPI interface.
The TI product page specifies a maximum frequency of 200 MHz, whereas the datasheet states a limit of 100 MHz.
Could…
Part Number: LSF0108 Other Parts Discussed in Thread: TXB0104 , TXB0106 Tool/software: As title, We want to confirm the LSF0108 whether SPI Quad mode is supported.
Thanks.
Leon Lin
Quanta BU9
Part Number: LSF0108 Tool/software: Hi,
What is the expected operation for the LSF0108 and other LSF translators if VREF_A is off (0V) and VREF_B & the EN pin are both at 3.3V? Would the B-side I/O be pulled down to GND, would the I/O be high impedance…
Part Number: LSF0102 Other Parts Discussed in Thread: LSF0108 , Tool/software: Hi team,
What's the difference between LSF0102 and LSF0108 in addition to channel numbers?
Part Number: LSF0108 Tool/software: Hi teams,
I was wondering if the A port and B port are open drain or push pull? Since I saw in the data sheet mentioned that they can have both open-drain and push pull application.
Thanks for the help!
Best,…
Part Number: LSF0108 Other Parts Discussed in Thread: TXU0104 , SN74AXC4T774 , SN74LV126A , SN74LXC8T245 , SN74LV125A , SN74LXC8T245-Q1 , Hi,
We are planning to use LSF0108QPWRQ1 for bidirectional GPIOs of our processor board, wherein each line can…
Part Number: LSF0108 Other Parts Discussed in Thread: TXU0304 , TXU0104 , TXU0204 , LSF0002 Tool/software: As shown in the figure above, we want to convert the 1.8V signal from the camera to communicate with the FPGA at 1.2V. In the figure, there is no…
Part Number: LSF0108 Other Parts Discussed in Thread: TXS0108E Hello All,
In some situations, I need the signal on both sides to be 3.3V. Will the LSF0108 work properly if VREF_A, EN, and VREF_B are connected to 3.3V?