Other Parts Discussed in Thread: LT1014 I am using LT1014 IC in a closed loop servo electronics to drive a load of maximum 8mA current. When I am testing this interface at low temperature especially below -15 deg Celsius, this interface output is showing…
Other Parts Discussed in Thread: LT1014 Does anyone know if the LT1014 has ESD diodes on each of the op-amps input pins? If so, how much current can enter these pins without damaging the op-amp. We have an unfortunate design where the inputs of the op…
Part Number: LT1014D Other Parts Discussed in Thread: LT1014 , SN74LVC1G74 ,
[Case:559816]Technical Data Inquiry
SiliconExpert is contracted our customer to work with its suppliers for accuracy and compliance purposes.
Could you please provide us…
Part Number: LF353 Other Parts Discussed in Thread: MC1458 , PGA204 , LT1013 , LT1014 , LM211 , LP211 , LM239 , LM3302
[Case:710026]Technical Data Inquiry
SiliconExpert is contracted by our customer to work with their suppliers for accuracy and compliance…
Other Parts Discussed in Thread: LT1014D , LT1014 We are using LT1014D: op-amp-1 and opamp-4 as inverting amplifier and opamp-2, opamp-4 are unused.
Using single power supply (+5V) VCC- terminal connected to GND
using op-amp-1 and op-amp-4 for monitoring…
Hamamoto-san,
Can I ask for a little more detail about why you want this capability? What type of condition are you expecting? Some op-amps will be able to support this condition and not break, but they will not operate properly. It is usually easy…
Hi Nathan,
Thank you for your post. If I narrow down our portfolio to 36V quad-channel precision amplifiers offered in a PDIP, we only have 9 parts:
OPA4277
OPA4131
LT1014D
LT1014
OPA404
TLE2024A
OPA4228
OPA4227
OPA4241
If you…
Hello Hac,
Our closest cross for the LT1007 is the OPA227:
Another possibility is the TLE2027:
For the LT1014 the OPA277 is suggested:
Regards, Thomas
PA - Linear Applications Engineering
Dear Bruce,
Thanks for the guidance. I think I was able to get to the source of my problems by following your comments.
I did the test you suggested, but the U2 output (3,1V DC) didn't change with variations of R4 (1k - 30k) nor with variations of…