Hi Donald,
The MAX3238E would be a pin-for-pin replacement to TRSF3238E with substantially lower output slew rate (since it was designed for maximum baud rates of 250 kbps). Based on the waveform you described (with fast rise times and slow decay),…
Vasu:
The MSP-FET430U100USB supports the F6659, but it is a "bare-bones" board. It brings out all of the I/Os to pins, so it would definitely give you the 30+ GPIO pins necessary. You would need to add support for the UARTs - there are no chips on the…
Other Parts Discussed in Thread: MAX3238 Dear all,
I want to ask whether the SCI-A port of the f28335 board can be directly connected to the PC DB9 port? What I mean is that whether the signal voltage transmit from the PC DB9 port is safe for the MAX3238…
Francisco Heredia said: Thank you very much for your response. I was able to solve this problem by skipping the TIUSB3410 and adding a MAX232 chip to the target board. I was able to get 230400 bauds from it. For faster speeds a MAX3238 is needed.
Francisco…
Other Parts Discussed in Thread: TMS320F28027 , MAX3238 I have two queries -
1. What are the programming options for Piccolo controllers? The only option I found was the Spectrum Digital programmers. Are there any other options?
2. My customer has made…
Part Number: TMS320F28335
Hi Sir/Mdm, I am trying to use RS232 cable to send and receive data through SCI-A (P12) and SCI-B (J12). However, the registers does not seem to be receive or sending any form of data. I am using a F28335 ezdsp. Anyone is able…