Part Number: TMP435 Other Parts Discussed in Thread: TMP423 , TMP451 Hi Team,
Do we have P2P compatible device with EMC1413-A-AIA-TR to recommend? Customer is looking for it. Attach is the d/s.
Best,
Stanley
EMC1413-A-AIA-TR.pdf
dear all,
I need to set the reference so that i get 80% duty cycle in the first phase. then i set the reference to 0 so that i get 0% duty cycle. But i do not understand how to calculate & set the reference.
i found that the output never falls completely…
Hi,
First as update, I changed the linux image to the one from the sdk. Thought there might be less problems like that.
Then, I received the log above when I loaded the firmware with the debugger (was probably lucky that it even did run, probably…
Part Number: PROCESSOR-SDK-DRA8X-TDA4X Hello!
I am trying to run Out Of the Box vision apps demos, followed all the steps as per this guide
( https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-jacinto7/latest/exports/docs/vision_apps/docs…
Part Number: PCM6020-Q1 Hello, Somebody help me.
I followed procedure in datasheet and set pcm6020 register like this. (i2c dump)
- Sleep -> Non sleep
- Power-up the ADC, MICBIAS, and PLL by writing P0_R117 - AC coupled, differential
and removed…
Part Number: TRF7970A Other Parts Discussed in Thread: MSP430F2370 Hi,
I am using TRF7970A to read MIFARE classic(1K) with 16 sector and 4 block in each. Want to read 16 bytes data of each block.
Is it compulsory to use direct mode to transmitting…
Part Number: BQ40Z60EVM-578 Other Parts Discussed in Thread: BQSTUDIO Hi,
Is there a doc outlining the setup for a 2S6P in the bqStudio using a bq40z60EVM-561:
2S6P
2 x 20400mAh
using Panasonic NCR18650B (?2012? four choices).
need something…
Hello Shravan,
We followed all the steps you mentioned. However we are still facing the same issue.
Attaching the logs for your reference.
We also checked the file "8233.0001-arm-dts-Update-timer-entries-for-remote-cores.patch.txt" you provided…
Thank you for your reply.
As I mentioned earlier, I want to send data from slave to master using SPI communication.
In CC430 SPI Slave code, start 0x0A hexa data and just increment it ;
And Cortex-M3 Master code, MCU receives the data from CC430…
Hi Norman and Titus,
I really appreciate the attention you guys have given to this issue.
Yes, this got to the point where things just didn't make sense. However, I am happy to say I've found the problem. Running the SPI transaction from spidev_test…