Part Number: MPY634 We attempted to assemble a wide-bandwidth multiplier, using your MPY634, but detected that its AFC was boosted with frequency (see table 1). Then we have assembled a test schematic in a prototype board with a MPY634 chip, just received…
Part Number: MPY634 I would like to use the MPY634 as a AM modulator. The circuit is wired exactly as mentioned in the datasheet figure 9 page 8.
Modulation input Em is + - 5V @ 150 Hz (square wave); Carrier input Ec= + - 8V @ 2 Khz (square wave) ;…
Hi Alice,
You did just fine with your English; multiplexer and multiplier are quite similar in their spelling and could be easily confused when English is not one's first language.
The MPY634 is a legacy analog function circuit. Burr-Brown introduced…
Part Number: MPY634 Can I know what would be the latency of analog multiplier MPY634 ?
Also can I multiply two signals of frequencies around 6GHz ?
Thank you.
Part Number: MPY634 Hi all Would you mind if we ask MPY634KP/KU? How much is the maximum TJ?(125C?) How much is the θja? We could not find it on the datasheet. Kind regards, Hirotaka Matsumoto
Part Number: MPY634 Hello,
I would like to know about MPY634KU, Wide Bandwidth PRECISION ANALOG MULTIPLIER operating temperature, it is mentioned as 'temperature range specification' -40 to +85Deg C.
Can we operate this at 100 deg ambient temperature…
Part Number: MPY634 Hi team,
My customer is wondering if we have analog multiplier with single power supply, +Vs(eg 15V), -Vs 0V ?
Could you please help to answer this?
Thanks.
Hello Oleg,
It appears that you are testing the MPY634 in a frequency doubling configuration with a very low frequency passive low-pass filter (-3 dB @ 16 Hz) following the output. I suggest testing the MPY634 by itself, without the input amplifier…
Hello Wojciech,
I could not replicate your problem with a MPY634 DIP and breadboard. Using your schematic, I connected the X and Z sources to DC power supplies and could see the part successfully divide the signals even for low signals such as (Z2…
Other Parts Discussed in Thread: MPY634 HELLO THIS IS HOT
I NEED TO NO IF THE PIN OUT IN THE DRAWING IS CORRECT
WHAT I NEED TO NO IS THAT IF I HAVE A SINE WAVE FEF. ON THE X (+) INPUT AND THE NEG. INPUT TO GROUND .
VOUT OF THE PART IS TIED TO Z1…