Hi,
Thanks for the links.
We can read faults after the next reboot when DSP is running since they are stored on Power Controller.
The following link contains PMBus Library but I'm not sure if its compatible with our HW.
www.ti.com/.../msp-pmbus…
Hi Siamak,
It's difficult to predict what the problem could be based on the information.
Is the MSP430 detecting a NACK because the slave device sends a NACK or is it sending a correct packet? Based on the information provided, it would seem like…
Hi Joscha,
the RTM for the LM51772 is planned for May/June timeframe and then full production volume would be available.
If you need more devices early please let me know.
An alternative solution would be to use the LM5177 and control the output…
Part Number: MSP430FR5969 Other Parts Discussed in Thread: TPS546C20A , , MSP430F5308 , MSP-FET Tool/software: WEBENCH® Design Tools We are building a power control board with a combination of "MSP430FR5969 + TPS546C20A".
However, we are using MSP430FR5969…
Part Number: UCD90SEQ64EVM-650 Other Parts Discussed in Thread: UCD90120A , MSP-TS430PEU128 I am prototyping some MSP430 code to interface with a UCD90120A device via eUSCI_B I2C. I have access to a UCD90SEQ64EVM-650 board with a similar UCD90120A device…
Thanks a lot for your swift answer.
My post over is unclear.
1. I do not want to solder. I want to buy a board.
2. The "break out all pins" board in the app note is some 89 USD. Too expensive.
3. I need only I2C and 2 digital pins (alert and…
Dear Jack,
Thank you for the link! I will try the updated UCD3138 code, because I think old one had some bugs (Write RAM to Flash and vice versa didn't work correctly even with GUI).
About MSP430 code that I am developing right now, I solved that problem…