Just a bit more information to be provided.
The steps I am using to update the firmware are as follows:
Start with the LP disconnected and GUI closed.
Open GUI/USB Firmware Update Example
Click "next" and agree to the license
Select specific…
Hi Krish,
Using 5V supply via USB should be sufficient for this, but there may need to be some iterations in power cycling to ensure the MSP is able to properly recognize the PHY. Previously, you had expressed difficulty in obtaining a 2.5V supply so…
Part Number: MSP-EXP430F5529LP Other Parts Discussed in Thread: DRV8323 Hello... I'm using an MSP-EXP430F5529LP MCU connected to a TI Motor Driver EVM (DRV83x3Rs), to spin a BLDC Motor.
For almost a year, the MCU, EVM and system worked flawlessly, while…
Hello Dennis,
Dennis Lehman said: Were you able to get the on-board eZ-FET recognized by windows device manager?
No Dennis, Windows is not recognized the on-board eZ-FET .
Instead of Communication port I got some Human interface devices as shown…
I connected the MSP-FET for the SpByWire more (just 2 lines and ground). CCS "found" it, and the software update to the MSP-FET went OK. It then took 2 tries to get it to recognize my PCB with the 430MSPFR2355, but it did download the program (and parts…
Can you change a cable?
It seems that CCS can recognize the MSP-FET, but the MSP-FET can't recognize the MSP430.
I advise you to capture the wave of JTAG pin. Maybe the cap at reset pin is too large.
Other Parts Discussed in Thread: ENERGYTRACE , CC2650 , MSP430F5529 , MSP430FG4619 , UNIFLASH Hi everyone,
this FAQ addresses the most common questions one might have about the new MSP432™ MCU. The main topics currently covered in this FAQs are:
…
Hello Cary,
Thanks for posting in this forum. Sorry you are having issues with the EVM connectivity. For further debug, switch off the VM motor power supply - not needed for USB enumeration for this EVM. You can turn this on after resolving the GUI…