Hi Eddie,
Thank you for your reply. That's possible, but all my writing environments use TI's tools.
- MSP-GANG
- MSP-TS432PZ100
- MSP-GANG-432ADPTR
I think TIer knows more about it.
I'll write other firmware (only to stop WDT) and check it,…
Hi Eddie,
Thank you for the reply.
>Can you provide the code? I need to ask my customer to provide the code. Is binary code will be fine or do you need c source code?
>What parameter settings are you using in the GUI? The only setup MCU category in…
Part Number: MSP432P411V Hello,
Does MSP-GANG support Flash writing for MSP432P411V? We think the combination of MSP432P411V, MSP-GANG-432ADPTR and MSP-TS432PZ100 should support MSP432P411V.
Also, does MSP-GANG-SOFTWARE support JTAG/SWD lock and IP Protection…
As I tried for some times, it works! Both with 20 pin on MSP-TS432PZ100 and 10 pin on launchpad.
Can you make sure the device is good, using XDS110 to check?
Hi Anthony,
Have you considered using the larger-memory MSP432P4111 device? It should be pin-to-pin compatible with the MSP432P401R that's on your LaunchPad. Alternatively, you could order the 100-pin target board, MSP-TS432PZ100. That should give…
Part Number: MSP432P4111 Tool/software: Code Composer Studio I've somehow managed to lose emulator connectivity with the MSP432 on three different targets.
I've bricked three boards that we designed for our application, but I've also bricked an MSP…
Hi Chris, I can check with my project manager the possibility to return some units. We bought 5 units. Four are fully destroyed, and the last one was not used yet. I really don't know what to do. At least, does the schematics seems correct? Asking…
We test 2 chips as in the photo. We still have the error.
We find an extra MSP432P401R from an other project. We have test it in the MSP-TS432PZ100 and it is working.
We came back to the 2 previous chips and still have the error.
Do you need any others…
Part Number: MSP432P4011 Hi, we build a custom pcb with MSP432P4011 rev A. Now I'm reading the docs of SimpleLink_msp432p4_sdk_3_30_00_13, specifically the 'Migration_Guide.html'. Now I get confused by:
IDE Requirements
When using the SimpleLink…
Hello Raghav
The LaunchPad is supposed to be an low cost evaluation board and it is not the intent to have every pin available on the header. You should be using the Socket Board for such application development.
www.ti.com/.../MSP-TS432PZ100