Part Number: MSP430F2252 Other Parts Discussed in Thread: MSP-FET Tool/software: Dear All,
Very good afternoon to all.
Task : We want to Flash .txt file in microcontroller MSP430F2252 using utility Command Line MSP Flasher with tool MSP-FET430UIF…
Part Number: MSP430F2252 Dear Sir - Hope you are doing well!
This is inline to my Case Number CS3078734.
We are currently using MSP430F2252IRHAR in our existing product, in-conjunction with external resonator of 1MHz with 1% accuracy. We are preseed…
Part Number: MSP430F2272 Other Parts Discussed in Thread: MSP430F2252 Hello,
We are using MSP430F2252 micro for our fire product and migrated from MSP430F2252 to MSP430F2272. The Micro(MSP430F2252) used to be upgraded by ATMEL MCU, means of BSL(UART…
Part Number: MSP430F2252 Tool/software: Code Composer Studio Dear Sir/Madam,
Regarding Port 2 interrupt.
Q1) Port 2.7 as interrupt :-
At initialization,
P2IE |= 0x80; // P2.7 interrupt enabled P2IES |= 0x80; // High to Low transition P2IFG &=…
Hi,
did you check out our code examples presented in the TI Resource Explorer yet?
You can just select your MSP430F2252 and browse for the Peripheral Examples on Register Level. There are several UART examples included which can help you to get started…
Hi,
Typically you could run the MCLK on a higher frequency to speed this up. However, it will also cost more power.
Additionally, you may use the IQmath library for MSP430 with the optimized Arithmetic Functions.
Part Number: MSP430F2252 I need to get MSP430F2252IYFFR ESD data include CDM/HBM. TI supprot team give me nothing and told me if follows
ESD control programs such as ANSI/ESD S20.20. I need to get real data, thanks !