Other Parts Discussed in Thread: MSP430F47167 Hi,
I am using MSP430F47167. I want to interface RTC using i2c module of it. After slave adress transmission the data does not trsmitt. I dont get any erorror flag set, it just wait for UCB0TXIFG to be se…
Other Parts Discussed in Thread: MSP430F417 , MSP430F47167 Dear Sir,
I have purchased a debugger from TI (MSP430-FETUIF) on before 4 years and started projects on same using controller
MSP430F417/169 it will ok to run.But now a days im working on controller…
Other Parts Discussed in Thread: MSP430F47167 I am using MSP430F47167. I am getting UCNACKIFG set after slave address sent ie. after
UCTXSTT setting and trasmitt flag dont reset on UCNACKIFG.
#include
"msp430x471x7.h"
uns…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
Aravind, The two microcontroller products that are included in the launchpad are these: * MSP430G2211IN14 – 2kB Flash, 128B RAM, 10 GPIO, 1x 16-bit timer, WDT, BOR, Comparator A+ * MSP430G2231IN14 – 2kB Flash, 128B RAM, 10 GPIO, 1x 16-bit timer,…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…
V6MSP430.dll.txt V7MSP430.dll.txt Hello Jace,
The first file is V6 DLL and second file is V7 DLL. I had to add the .txt extension since uploader won't allow .dll
Dave