Other Parts Discussed in Thread: MSP430F5338 , CC3100 Hey,
I'm working with MSP430F5338 and trying to set a UART connection with another component (TI CC3100) with the following configurations:
Baud rate: 921600 [bps]
Data bits: 8 bits
Flow control…
Other Parts Discussed in Thread: MSP430F5338 , CC3100 Dear TI members
My HW setup consists of CC3100 and MSP430F5338, we are planning to integrate an OTA solution with CC3100 SDK.
From the latest CC3100 SDK AN and another thread from the CC31XX forum ( …
Other Parts Discussed in Thread: MSP430F5338 Hi,
I have problem with MSP430F5338. I need set up timer to generate interrupt at the exact time. For example i need generate interrupt with frequency 1.5 , 2 , 2.5 , 3 , 3.5 (20,50-100Hz etc... ) Hz.
Clock…
Other Parts Discussed in Thread: MSP430F5338 I've got a MSP430F5338 acting as a I2C slave in a design and I have a question about the order of the interrupts that the USCI module generates.
The master is sending two bytes, 0x02 and 0xa5 to the MSP…
Other Parts Discussed in Thread: MSP430F5338 Hi,
We are using :
1. Target : MSP430F5338
2. TI-RTOS ver# 1.21.00.09
3. IDE : CCS Version: 5.5.0.00077
There is no hardware support for UART (serial) flow control (RTS and CTS) in MSP430F5338. Does TI-RTOS…
Other Parts Discussed in Thread: MSP430F5338 Hi,
I am using MSP430F5338 and I am using ADC12 module. When configuring ADC12 module, I configuring VREF+ as AVCC and VREF- as AVSS, hence I have P5.0 and P5.1 free to use as GPIO. When I write P5SEL bit 0…
Other Parts Discussed in Thread: MSP430F5338 Hello
I am using MSP430F5338 UART OF USCI_A0.
I have configure Port 2 pins for TX and RX using PORT mapping functions.
I have used ACLK 32768hz.
I want to transmit only one byte on uart . But my code is not…
Hello
I am using msp430f5338 in my current design.
I am trying to write data in flash with following function
void write_flash_seg(unsigned int* addr,unsigned int value) { unsigned int *Flash_ptr; // Flash pointer Flash_ptr =addr; while(FCTL3 & BUSY…
Other Parts Discussed in Thread: MSP430F5338 , MSP430F5438A Hello
I am using MSP430F5338 in my design.
I am sending array of bytes to a module and in response module also sends array of bytes.
I am able to receive that array but in that some bytes are missing…
Other Parts Discussed in Thread: MSP430F5338 Hello
I am using MSP430F5338 in my design.
I am using I2C and UART communication.
I2C is running by SMCLK and UART is ACLK . Source of clock is REFOCLOCK for both.
When UART is off then I2C is working fine. …