Other Parts Discussed in Thread: MSP430F5505 Hi!
I'm using a MSP430F5505 with a 32768 Hz quartz on XT1.
I want to use 2 external load capacitors instead of selecting internal capacitors with XCAP.
Therefore I would clear XTS in UCSCTL6. Is it…
What consideration have you given to the MSP430F5505? It has USB. I've attached a comparison with the differences highlighted in yellow.
3058.msp430 comparison.xlsx
MSP430 USB Developers Package would be available to you to use if you select a MSP430…
Hi,
yes! You can! Find the description from the elprotronic website below:
Rgds aBUGSworstnightmare
Supports in fully TI's PP, USB FETs and
EZ430
only.
Includes TI's MSP-FET430UIF
firmware update. Communication via JTAG and Spy-Bi…
I do not understand why you want that.
As far as I know, there is no errata for the following members yet.
MSP430F5500, MSP430F5501, MSP430F5502, MSP430F5503, MSP430F5504, MSP430F5505, MSP430F5506, MSP430F5507, MSP430F5508, MSP430F5509, MSP430F5510…
Other Parts Discussed in Thread: MSP430F5505 Hi everybody.
I'm using timer A 0 (of a MSP430F5505) in contious mode with 4 channels. I want to generate indipendent time intervals.
I start the timer with this function:
void StartTimerA0() { TA0EX0…
Hi zohar,
thanks for your reply.
I was comapring the two processors, and it tseems that the only differece is the number of GPIO, the package, and the number of USCIs (I2C/UART/LIN/IrDA/SPI)
http://focus.ti.com/paramsearch/docs/compareresults…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…