Hi,
yes! You can! Find the description from the elprotronic website below:
Rgds aBUGSworstnightmare
Supports in fully TI's PP, USB FETs and
EZ430
only.
Includes TI's MSP-FET430UIF
firmware update. Communication…
I do not understand why you want that.
As far as I know, there is no errata for the following members yet.
MSP430F5500, MSP430F5501, MSP430F5502, MSP430F5503, MSP430F5504, MSP430F5505, MSP430F5506, MSP430F5507, MSP430F5508, MSP430F5509, MSP430F5510, MSP430F5513…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
Other Parts Discussed in Thread: MSP430F5438A , CC1120 , MSP430F5506 , MSP430WARE Hi!
I have a question regarding the communication between the CC1120 and my MSP430F5438A on my CC1120 DK kit. I am currently developing software for my future MSP430F5506 processor…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…
V6MSP430.dll.txt V7MSP430.dll.txt Hello Jace,
The first file is V6 DLL and second file is V7 DLL. I had to add the .txt extension since uploader won't allow .dll
Dave