Thanks for the quick reply. The code has samples for D/A converter not for A/D converter. The IAR workbench has in his device list only an msp430F6630, not msp430fg6626.
Could this be a problem or will?
Thanks.
Other Parts Discussed in Thread: MSP430F6638 , CODECOMPOSER , MSP430F6630 Hi Everyone,
I need to write a simple function generator for my MSP430F6638 MCU. Does anyone have any sample code?
Thanks,
Arash
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
Hi Conor,
I look through the errata of this MCU. And find the PORT17 similar to your scenario.
If there is negative high current goes into the P6.2, it could cause the adjacent pin (P6.3 A3) latch-up in some cases. You can find more details through…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
Hardy,
The first device in the F5xx family that will have a DAC is the F56xx/F66x devices.
These will sample in a month's time (July 2010) and be ready for the market in late 2010.
If you needed samples before then you can contact Les Taylor…
Hi Akash,
The erase check and TX BSL version commands are members of the standard command set in BSLs V1.50 or higher but excluding 2.x BSLs. The MSP430G2544 is BSL Version 2.02, ergo no TX BSL version command support for this device.
You can go through…