Part Number: MSP430F6636 Tool/software: Code Composer Studio Hello,
I have created a ProjectSpec for MSP430F6xx that needs to have the erase option, "Erase main and information memory", enabled by default, instead of the Erase memory only option. Is this…
Part Number: MSP430F6636 Tool/software: Code Composer Studio Hi,
I have some issue with my ADC. I don't know why the reading is wrong, my input is 1000mV the ADC = 1675 => 1022mV and bounce between 1001-1015mV. When I pause the code the mV is…
Part Number: MSP430F6636
Tool/software: TI C/C++ Compiler
Hi,
I have problem with calloc function :
ptr = (int *) calloc(200, sizeof(int));
for(i=0; i<200; i++) {
ptr[i] = i+1;
}
When i compile the code and debug…
Part Number: MSP430F6636
Tool/software: Code Composer Studio
Hi,
I don't know why but my CCS ver 7.0.0.00042 don't detect missing semicolon in my header file. When i try compile the code i get 100 errors in 5 different files except missing semicolon…
Other Parts Discussed in Thread: MSP430F6636 Hi,
Can you please share if any of your client has used C# to communicate with HID class as host USB. We are using MSP430F6636 as a device.
We need C# example urgently for our application development. We are…
Other Parts Discussed in Thread: MSP430F6636 , MSP430F6634 Where I can see the maximum current of DVCC and AVCC in MSP430F6636?
Is there another version instead of MSP430F6634 that has a capability of 5V on the LCD pins?
Is there another version instead…
Other Parts Discussed in Thread: MSP430F6636 , TRF7970A What is the recommended connectivity of the SYS_CLK and DATA_CLK lines of the TRF7970A with MSP430F6636?
The MSP430F6636 is used for additional applications (USB, clock in LCD,...)
Other Parts Discussed in Thread: MSP430F6636 Hello All,
I'd appreciate some guidance with using the LCD_B Controller and the MSP430F6636 to drive an 80-segment LCD (2_Mux).
This is my first attempt at using a multiplexing LCD controller, and i am not…