Hi,
It is possible that it is just MSP430F6658.
I think you can set it as MSP430F6658 first, and check the TLV data.
If the device ID is not 8286h but 812Ch, there are two possibility:
1. It is just F6658
2. You have changed the data in Device…
After researching the web site more, I see the source code for the USB BSL function may be available for the MSP430F6659. Can someone point me to it? Also, I'm confused by the comment in the slau319 Table 36(below) that says " Factory USB BSL is RAM write…
Part Number: MSP430F5659 Hi all,
We have concern about one of your devices, microcontroller MSP430F5659IZCA.
We’ve just added it to our manufacturing process due to a obsolescence of MSP430F5659IZQW.
However, the datasheet doesn’t specify the type…
Other Parts Discussed in Thread: MSP430F6659 , MSP430F5358 , MSP430F5359 , MSP430F5658 , MSP430F5659 , MSP430F6458 , MSP430F6459 , MSP430F6658 Hi,
anybody used successfully the MID (memory integrity device) on an MSP430F6659 Rev A?
On my MSP430 dumping…
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
Can someone from TI give me an idea on when samples for the MSP430F5658IPZ or MSP430F5659IPZ (or the F665X versions) will be available? (in the 100 pin LQFP packages)
I have a development board I am close to building with the 5638 and it would be nice…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest software…