Other Parts Discussed in Thread: MSP430F6723A , MSP430F6723 Hello
I selected the MSP430F6723A for new project.
But I can’t find the difference between F6723A and F6723.
They almost have the same specifications.
Do anyone kindly to tell me? …
Part Number: MSP430F6725A Other Parts Discussed in Thread: MSP430F6723 , MSP430F6723A , , UNIFLASH , MSP430F6730 , MSP-FET Tool/software: Code Composer Studio When installing the MK (MSP430F6725A IPN (TI) on the device card in replaceable MSP430F6723A…
Hi, No, PMM will not work, please see the Table 5-12 in chapter 5.8.5. msp430f6736a.pdf The test conditions is | dDVCC/dt |<3 V/s, 3V/5ns drop too fast. But I can't give an exact answer what the performance of MCU when it drop below 1.8V at a rate of…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest software…
Hi Paul,
I use the MSP430 product selection page from https://www.ti.com/microcontrollers-mcus-processors/msp430-microcontrollers/products.html and save all parts in the spreadsheet. I use the filters to filter out parts. There are quite a few that…
Hi Akash,
The erase check and TX BSL version commands are members of the standard command set in BSLs V1.50 or higher but excluding 2.x BSLs. The MSP430G2544 is BSL Version 2.02, ergo no TX BSL version command support for this device.
You can go through…
Other Parts Discussed in Thread: CC2640 , CCSTUDIO , CC2538 CCS not detecting installed compiler tools in Windows Docker container for CI build Hello all BACKGROUND: I'm trying to set up a CI build for a CC2640 processor using a Windows Docker container…