Let me explain what I was asking.
MSP430F67461 is an I/C. Without any external hardware , it looks like this.
You said you are using JTAG to debug it already. To me, that means you already have some external hardware that let you connect the MSP430F67461…
Hello JH, Many thanks for your reply i have another question my company changed the controller to be msp430f67461 is that controller supported by TI energy library ? If yes please tell me how to configure the channels for the volts and the currents because…
Some additional insight on the front end of this discussion:
We do have some MSPs with more than 3 independent SDs. I think the family you should look into are the F67xx1 devices which are normally utilized for metrology applications.
The MSP430F67461…
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest software…
Hi Akash,
The erase check and TX BSL version commands are members of the standard command set in BSLs V1.50 or higher but excluding 2.x BSLs. The MSP430G2544 is BSL Version 2.02, ergo no TX BSL version command support for this device.
You can go through…