Hi Akash,
The erase check and TX BSL version commands are members of the standard command set in BSLs V1.50 or higher but excluding 2.x BSLs. The MSP430G2544 is BSL Version 2.02, ergo no TX BSL version command support for this device.
You can go through…
Hi Paul,
I use the MSP430 product selection page from https://www.ti.com/microcontrollers-mcus-processors/msp430-microcontrollers/products.html and save all parts in the spreadsheet. I use the filters to filter out parts. There are quite a few that…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use the…
V6MSP430.dll.txt V7MSP430.dll.txt Hello Jace,
The first file is V6 DLL and second file is V7 DLL. I had to add the .txt extension since uploader won't allow .dll
Dave
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );
Which…