Part Number: MSP430F6766 Hi Experts,
I am helping a customer trying to find a Microcontroller or Processor that can run for 28 days on 3 D cell Alkaline batteries. Capturing a 24Bit ADC onto an SD card. Can you please also advise on a few options? I was…
Hi,
What is "TRM"?
If you are meaning data sheet I have, please see attached datasheet. it was downloaded when I was developing firmware.
msp430f6766.pdf
Best Regards,
Elly Lee
MSP430x6 Family User Guide.pdf
Other Parts Discussed in Thread: MSP430F6766
Hi,
I am using MSP430f6766 and trying to get the RTC (RTC_CE) value on the LCD. I could able to display the RTC values (time ,date, month and year)
properly. However when I am turning off the system (Power…
Other Parts Discussed in Thread: MSP430F6766 Dear All,
I am working on 3-phase energy measurement application using MSP430F6766. Can anyone please tell me from where I can get the Code Composure Studio supported 3-phase energy measurement library?
Thanks…
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest…