Other Parts Discussed in Thread: MSP430F67751 , MSP430F6638 I'm using THE MSP430F67751 Controller with XT1 Reference Clock of 32.768 kHz.
I can measure 32.767kHz at the ACLK Output.
The PLL-Ratio is 512 and should give me 16.777 MHz.
However the measured…
Other Parts Discussed in Thread: MSP430F67751 Hi All,
I am trying to calibrate the RTC C for the crystal offset error. I have a 32khz clock for the XT1, Main clock frequency is 16MHZ. micrcontroller msp430f67751.
Questions:
The calibration procedure in…
Other Parts Discussed in Thread: MSP430F67751 What is maximum voltage of AUXVCC3 for MSP430F67751 , If I am using 3.3V will controller fail? What are the consideration if use AVCC, DVCC, AUXVCC1 and AUXVCC3, Is there any setting to be required to use those…
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest…