There is so little on actually writing to a specific address, its shocking.
My problem is I want to write and then read back that value to see if communication is successful, however, once written the address pointer increments by 1 so isn't the same…
Hi Jack,
You can change the target device in the project properties menu in CCS. In the project explorer on the left hand side, right click the project name, and select Properties. In the General section, in the Main tab, you can change the variant…
Other Parts Discussed in Thread: MSP430F6779 , MSP430F67791 , MSP430F6779A Some MCU ' s on same family, has suffix for example "1" or "A".I wonder what is it means.For example:
msp430f6779
msp430f67791
msp430f6779A
What is the difference of these…
Hi Ryan,
Changed to RTCCTL0_H = RTCKEY; with no luck.
I haven't set any timers or anything and I am using the MSP430F6776 so don't have to set any ports for the XTAL, but I thought that wouldn't effect writing to the RTCSEC register etc.
Jac…
Other Parts Discussed in Thread: MSP430F6776 Hi,
I am using EVM430-6779 but I am not use that code for another design using the smaller MSP430F6776, how do I update the code so that the correct include file is used?
Thanks
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"