Other Parts Discussed in Thread: MSP430FG439 Hello Eveyone,
I am somewhat confused about how do the port configure itself for the alternate function.
for e.g: MSP430FG439 P6.3 has alternate function for ADC as well as for OPAMP input/output
by selecting…
Other Parts Discussed in Thread: MSP430FG439 Hi;
I worked on the msp430fg439 and it has only one spi channel and i used sd card interface at this spi channel pins. I have to use 3310 lcd but it works spi interface. I have extra 8 digital pins (not spi…
Other Parts Discussed in Thread: MSP430FG439 Hello everyone,
I have to implement three op amp instrumentation amp using msp430fg439 with gain of 93.
so how can we implement it using OA0,OA1 OA2 and OAFBRx register.
thanks
asma
Other Parts Discussed in Thread: MSP430FG439 , CC2650 So I am currently working on a fitness device that uses the CC2650 Bluetooth module(this module interacts with your smart phone), the MK-II booster pack(this displays the pedometer part of my project…
1. Yes, it should be no problem.
2. No, MSP430FG439 doesn't support flow control. However, I don't think it is a problem in your application.
3. You can try to output data from UART on Coordinator.
Other Parts Discussed in Thread: MSP430FG439 Hi Team,
I have few questions about a clock system in msp430fg439, could you please check the below questions?
1. Accuracy of 4MHz DCO using FLL with 32768Hz on XT1, FN_3(Typical DCO range 2MHz to 17.9MHz…
Hi Adrian,
This thread discusses some GSM modules which have been interfaced to our MSP via a UART AT Command set:
https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/220652…
Other Parts Discussed in Thread: MSP430FG439 Hello Everyone,
I am using MSP430FG439 i want to continuously sample two channels A0 and A1. I am getting the data from this two channels properly. but i want to increase sampling speed from 5Mhz(ADC12OSC…
Other Parts Discussed in Thread: MSP430FG439 Hi,
I recently started using the MSP430 Launchpad and I want to know if there were any MSP430s with internal opamps but in a DIP package that could be programmed using the emulator on the launchpad.
I basically…
Other Parts Discussed in Thread: MSP430FG439 Hello Everyone, I am using Olimex JTAG LPT debugger.....and i have mod pulse development which contain MSP430FG439.... this debugger is not able to program this IC. It is showing me this error.
Wed Nov 27…