On the data sheet I see pin 96, RST(active low) listed as "I/O". Is it possible to write to this pin and force a reset. We have external hardware hooked up to this that needs to be reset. I tried a watchdog reset but that did not affect the…
Other Parts Discussed in Thread: MSP430FG6625 , MSP430F5510 , MSP430F5659 Hi,
I have a question regarding the 24Mhz clock which I am getting it from external XT2 cristal. I configure my code to use 24Mhz XT2 as the main clock for SMCLK and MCLK. I also verified…
Other Parts Discussed in Thread: MSP430FG6625 We're using the MSP430FG6625 microcontroller and need adjust VCORE.
The MSP430x5xx and MSP430x6xx Family Users's Guide provides some guidance and also references SLAA448, however all the links I find to…
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…