Part Number: MSP430FR5947 Other Parts Discussed in Thread: UNIFLASH , MSP-FET , Tool/software:
Hi,
We are performing production programming of MSP430FR5947IRHA devices using ELPROTRONIC's GangPro-430 programmer (Spy-Bi-Wire interface), and encountering…
Part Number: MSP430FR5947 Installed CCS 11.2 on Windows 11 ARM (on Parallels 18 on Mac M1 Max) is failing to install.
Specifically the installer gets to the stage where it tries to install certificates (and succeeds) and then attempts to install the…
Part Number: MSP430FR5947 Other Parts Discussed in Thread: MSP430FR5949 I am using MSP430FR5947 controller (38 pin, DA Package). As both MSP430FR5947 and MSP430FR5949 are pin to pin compatible, the only difference is FRAM size and location.
1. In MSP430FR5949…
Other Parts Discussed in Thread: MSP430FR5947 I am using MSP430FR5947. I want to initialize all the peripherals using Grace software. But MSP430FR5947 is not available in present Grace software. I wanted whether this controller can be initialized through…
Part Number: MSP430FR5947 Other Parts Discussed in Thread: MSP-FET I get an MSP430Flasher.exe error code 59 when writing to MSP430FR5947 BSL area ???
Please can you help
Thanks
Richard.
Background: Evaluating MSP-FET programmer for use on project…
You can use the MSP-TS430RHA40A EVM, the only difference is that pin 30 does not require the 470 nF pulldown capacitor connected to it (C9) as the MSP430FR5947(1) devices do not have a VCORE. All other pins line up correctly. You can use a MSP-FET or…
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest software…