Other Parts Discussed in Thread: MSP430G2111 Quick question about the MSP430G2111, Can I just hook it up to a FTDI chip or do I have to buy a launchpad? (i know you can get the schematics for the launchpad but i need something fast for prototyping).
Other Parts Discussed in Thread: MSP430G2111 I have an Arduino and an MSP430G2111. I was wondering if it is possible to program the MSP430G2111 through the Arduino. I am on a strict budget so i opted to not buy the launchpad and see if ICSP was an option…
Other Parts Discussed in Thread: MSP430G2111 With the MSP430G2111, is it possible to program a cap value for PWM or is the max set at VIN and you have to use an analog to digital converter, send the output to an op amp, then through a digital to analog…
Other Parts Discussed in Thread: MSP430G2111 , MSP430G2131 Greetings,
Can you please provide a simple explanation of the difference between the MSP430G2111 & MSP430G2131 A/D option, the difference between a Slope versus 10-bit SAR ADC. I assume the…
Hi
I would like to config timer A1 to output ~4Khz square wave on P1.6 using CCR1 (no interrupt, no CPU load) and 125 msec interrupt using CCR0
I have manage to produce the 125 MSec interrupt by configuring the following register's :
CCTL0 =…
Ashutosh,
1. I'm a little confused as to what your asking. A power on reset (POR) can be generated in 3 ways: Powering up the device, pulling the RST/NMI pin low, or by an SVS low condition with PORON=1 (essentially meaning a drop in supply voltage…
Hi Louis,
the lastest SW-version for MSP430-GANG ( http://focus.ti.com/docs/toolsw/folders/print/msp-gang430.html ) is V1.51!
This version has support for new devices: MSP430F5513, MSP430F5514, MSP430F5515, MSP430F5517, MSP430F5519, MSP430F5521…
Hi Miles,
I recommend using the MSP430 product selector http://focus.ti.com/paramsearch/docs/parametricsearch.tsp?&familyId=342&uiTemplateId=PP-T-GSPA_T&techFamId=null&rootFamilyId=null§ionId=95&tabId=1200&appId=null&viewDeviceCallingPage=null&totalCount…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…