Other Parts Discussed in Thread: MSP430G2452 , MSP430G2352 Hi,
below is the partial code that i am working on:
#include <msp430g2452.h>
void main(void) { WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer P1DIR = 0x07; // P1.0 output, else input P1OUT…
Dear all,
I have the same problem as mentioned above. I'm using the MSP430G2352 Controller and IAR Workbench 5.40.3 with TI-MSP430 FET UIF.
Please advise .
best regards
Ulli
Matt Shira said:
... the board has its own 1.8V power supply...
I would caution against powering your MSP430G2302 with 1.8 V for a few reasons:
Tolerance. What is the tolerance of your 1.8 V supply? 1.8 V is the minimum supply voltage for the MSP430 …
Hello
I recently started to work with MSP430, and trying to run a simple program on Launchpad with MSP430G2352 .
I was able to write what I need without using interrupts and low-power mode. But to move further I need to implement both.
When I am trying…
Other Parts Discussed in Thread: MSP430FR5949 Dear Sirs I need your help for an application I'm developing. The MCU is a MSP430G2352 and I have some doubts with the use of the Watchdog. Here attached there is the code (without of all unecessary stuff…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…