Part Number: MSP432-RTOS Tool/software: TI-RTOS Hello!
I have NFC bank card reader, it uses RS232 and PPP to connect to bank host. Also i have SIM800 for internet connection.
I want to use MSP432 between NFC-reader and SIM800 as a UART-TCP/IP converter…
Part Number: MSP432-RTOS Other Parts Discussed in Thread: PCF8575 Hi folks!
I use I2C (100/400 KHz) within POSIX/TI-RTOS (SL SDK 3_30) talking without problems to couple of I2C IO expanders PCF8575.
Driver usage is like SDK examples for I2 master…
Part Number: MSP432-RTOS Other Parts Discussed in Thread: SYSBIOS Hello,
I have a few tasks that sometimes fail (forever) to wake up. If I break execution, I see the idle task's stack. How do I switch TCBs to do a backtrace on another task?
Latest…
Part Number: MSP432-RTOS Other Parts Discussed in Thread: CC3120MOD , BOOSTXL-AUDIO , CC3120 Hello,
I am working on a college project where I want to use the CC3120MOD along with the BOOSTXL-AUDIO to wirelessly transmit sampled audio data using an MSP432P401R…
Part Number: MSP432-RTOS Tool/software: Code Composer Studio Dear all,
I cannot get my SD card running using “fatsd_MSP_EXP432P401R_freertos_ccs”.
SD card
As indicated in many Q&A on forums I have the following:
3.3V --> msp3.3V,
GND --> mspGND…
Part Number: MSP432-RTOS Hi Folks,
I am using device having MSP432P401 uc which is running FreeRTOS application. I have following configuration to run the device at 48MHz.
PowerMSP432_PerfLevel MyCustomPerfLevels = { .activeState = PCM_AM_DCDC_VCORE1…
Part Number: SIMPLELINK-MSP432-SDK Other Parts Discussed in Thread: MSP432E401Y , SYSCONFIG Hi,
I've imported the fatsd and fatsd (the "no rtos" ones) for MSP432E401Y from ResourceExplorer and made the necessary SPI connections with a SD card reader…
Part Number: MSP432-RTOS Hello,
I am trying to run the sample code from the project rtc_c_calendar_alarm_interrupt_MSP_EXP432P401R_nortos_ccs ( https://dev.ti.com/tirex/explore/node?node=AJqwjKihbubkqdiKJIzyVQ__z-lQYNj__LATEST ) from an RTOS environment…
Part Number: MSP432-RTOS Hi,
I tried dynamic memory allocation using malloc(1024 * 24), but failed.
For sure, I reduced its size to 9K bytes and found it is the upper limit as of my project in CCS.
Following is the capture of Memory Allocation view…
Part Number: MSP432-RTOS Tool/software: Code Composer Studio hello sir
I have to ask one thing , is there any board of msp432 series has uart i meant extra USB port?"