Part Number: TMS570LC4357 Other Parts Discussed in Thread: HALCOGEN Tool/software: Code Composer Studio
Hi,
When I tried to test sefeti-lib, I encountered such a compilation problem. How can i fix it?
Thanks a lot
B.R
Y.L
Hi Ilija,
I compared your project with safety diagnostic project that i had and i don't see the inclusion of the libraries "SafeTILib_RM44_LE.lib" and "F021_API_CortexR4_LE_V3D16.lib"
Are these libraries are required for your application…
Hi Strong,
We don't have an official EABI version released currently, but I did put together an FAQ thread with some guidance on how to migrate it from COFF to EABI:
https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f…
Hi Samuel,
The User's Guide in the "docs" folder of the diagnostic library contains guidance on using the library. The difference in the two .lib files is that the "debug" version is built with optimization turned off and ASSERTs (used for parameter checking…
Dino,
the above block diagram is a copy from the TIDA-01599 design guide. The power stage can TIDA-00995, but is not limited to that. We can use other and newer CMOS gate drivers such as UCC21750 or simple gate drivers like UCC53XX.
The TIDA-010599 used…
Part Number: TMS320F28P659DK-Q1 Tool/software: When integrated P65 secure boot related code into our project which has implemented Safety diagnostic library. A conflict happens between two libraries.
f28P65xCPU1_SecureZoneCodeSymbols_fpu32.lib(Use-…
Hi Ethan,
I think the best place to start is with the F28377D safety manual and this IEC 60730 / UL 1998 overview for C2000 devices . The safety manual describes the safety features and diagnostics (both hardware and software) for the device and the overview…
Part Number: LAUNCHXL-F28379D Other Parts Discussed in Thread: C2000-SAFETI-DIAGNOSTICS-LIB , C2000WARE Hello! I recently downloaded the ‘ C2000-SAFETI-DIAGNOSTICS-LIB — C2000 SafeTI Diagnostic software library with Compliance Support Package…
Hi
Thanks for your information. I am using F28379D for my product design and format is EABI. I were download C2000-SAFETI-DIAGNOSTICS-LIB and found it is in COFF.
I tried to convert library from library source code to generate EABI format. However, I…