Part Number: MSPM0G1105 Hi,
We would like to ask for your support regarding a programming issue we are experiencing.
Programming failure during software write
When programming the device using MSP-GANG Programmer, the programming process…
Part Number: MSPM0G1105 Hello,
I have a customer who suspects that unstable ADC readings are causing failures in their PCB verification tests. I have suggested the following to try to stabalize their ADC readings:
Perform HW averaging
Increase…
Part Number: MSPM0G1505
I'm trying to understand more about the "Tsample_PGA" specification for the MSPM0G ADC when used with the internal op-amp. These sampling times are much longer than those for the ADC alone.
Am I correct to believe that this…
Part Number: MSPM0G1105 Hi, customer started a project from our SDK examples. Now he wants to use VCS tool but don't want to check in the complete SDK but the needed files including the linked (header and lib) files. Is there a automated process to get…
Part Number: MSPM0G1105 Hi All,
It was stated that in order to unlock the CPU, it is necessary to connect in BSL mode and then rewrite the device again via SWD.
MSPM0 NONMAIN FLASH Operation Guide
I am considering connecting via UART to enter…
Part Number: MSPM0G1105 Tool/software: Q1) Trying to find an MSPM0G MCU which can drive CLK_OUT at 32MHz at 1.8V, but everything I can find seems to show I need VDD > 2.7V to drive at 32MHz. Is there such a part, or is CLK_OUT pin a special driver with…
Part Number: MSPM0G1105 Other Parts Discussed in Thread: LP-MSPM0G3507 Tool/software: Hi All,
1) Is the connection between the XDS110 and the microcontroller correct? Microcontroller XDS110 (CTI20) SWDIO (34-pin) ⇔ SWDIO/TMS (1-pin) SWCLK (35-pin) …
Part Number: MSPM0G1105 Other Parts Discussed in Thread: MSPM0G3507 , , AM5708 , SYSCONFIG Tool/software: A few months ago, I made an engineer sample and connected the resonator (ceramic resonator) to the HFXT,
but the amplitude was not the expected…
Part Number: MSPM0G1105 Tool/software: Hi All,
Could you please answer this question.
MSPM0G1105: Unable to write data to the specified address using MSPGANG_Interactive_WriteBytes_to_FLASH(). - Arm-based microcontrollers forum - Arm-based microcontrollers…
Part Number: MSPM0G1105 Hi, customer uses CCS v20.4 and try to compile and link a project using the GNU ARM toolchain (arm-none-eabi-gcc/g++). Does CCS 20.4 support the use of the GNU ARM toolchain for C++ projects (including automatic selection of the…