Part Number: MSPM0G1507 Tool/software: I have a question regarding the programming process for the TI MSPM0G1507 microcontroller.
Is it not possible to reprogram the hex file directly without needing to invoke the BSL?
Additionally, do we need to…
Part Number: MSPM0G1507 Tool/software: I am developing a flash programmer for MSPM0 that runs on a Teradyne In-circuit tester that runs through the SWD.
I have successfully developed this Flash Programmer for the MSPM0G1507. It works fine for 2 of 3…
Part Number: MSPM0G1507 Tool/software: Hello,
I am sampling the temperature sensor on the MSPM0G1507 and I am having some issues when converting the ADC reading to a temperature. My ADC values on ADC0 channel 11 (Temperature Sensor) are around 1760…
Part Number: MSPM0G1507 Tool/software: Hi Team,
One of our customer meet two problems when they build project based on CCSv20.0.3. As they reported, it seems a CCS environment setup related issue, and not related to there code. Could you please help…
Part Number: MSPM0G1507 Other Parts Discussed in Thread: LP-MSPM0G3507 , , MSPM0G3507 Tool/software: Hi TI Community, I am facing an issue during board bring-up and would appreciate your insights. I successfully developed and tested an I2C firmware on…
Part Number: MSPM0G1507 Tool/software: Hi,
Unfortunately we have broken the adapted to debug the Board.
Do you have an schematics connection of that adapter.
Th adtapter is the one from
“ Compact TI 20-Pin (cTI) 2” TO “ ARM 10-Pin 3”
https…
Part Number: MSPM0G1507 Tool/software: Hello,
Just wanted to confirm the behavior of the flash module when performing a program/ erase operation. In section 7.2.1 of the TRM it states that all read requests on the same bank would stall until the operation…
Part Number: MSPM0G1507 Tool/software: Hi All,
I have some questions about the datasheet.
1.When a GPIO port is set as an open drain port, is there any problem if an intermediate potential is applied to the port? (Through-current flows, etc.) 2.The…
Part Number: MSPM0G1507 Tool/software: Hello TI Experts,
According to Table 7.16.4, the DAC has an offset error of ±20 mV without calibration or ±2 mV with calibration. Is this offset considered part-to-part variation, or can it also drift on the same…
Part Number: MSPM0G1507 Tool/software: Hello,
according to register description in the MSPM0 G-Series Technical Reference Manual, the DAC's CALCTL.CALSEL selects the Factory Trim Calibration Values after reset as default. The manual doesn't mention…