Part Number: MSPM0L1227 Other Parts Discussed in Thread: SYSCONFIG Tool/software: Hi,
My customer wants to change the stack size from the default number “256”.
Could you tell them how to change the stack size ?
They tried to add “-stack size=0x580…
Part Number: MSPM0L1227-Q1 Tool/software: Hi,
I wonder whats the range of pullup- and pulldown-resistance for GPIOs is.
In the datasheet SLASFB5A, november 2024 page 52, only the typical value of 40kOhm is listed.
Part Number: MSPM0L1227 Other Parts Discussed in Thread: UNIFLASH Tool/software: Hi,
My customer has a question below. Could you answer their question ?
The following error occurred at the Flash Read. Do you have any idea to solve this ?
Source…
Part Number: MSPM0L1227-Q1 Other Parts Discussed in Thread: MSPM0L1227 , MSPM0G3519 , MSPM0G3507 , MSPM0L1306 Tool/software: Hi Team,
Do we have an example code for communication SBC TLIN1431 with MSPM0L1227 over SPI with CRC feature enabled?
Thank…
Part Number: MSPM0L1227-Q1
Hi Experts,
We faced the FLASHDED error when we access to BANK1 during running the application on BANK0.
Now we are implementing the backup function of BANK1 during running the application on BANK0. But the FLASHDED error…
Part Number: MSPM0L1227 Tool/software: Hi,
My customer has some questions about Maximum number of write operations NW(MAX) described in the table of 7.8 Flash Memory Characteristics in the datasheet.
If it moves to another word line in the same…
Part Number: MSPM0L1227 Tool/software: Hi,
My customer wants to update (Erase and Write) some data in Flash during user application running.
Could you tell them how to do that ?
In order to erase/write the data in Flash, they’re thinking to…
Benjamin Steiner said: Datasheet says, the POCI (MOSI) would be forced Low while in Idle.
Also in your picture the signal goes High.
Is the datasheet wrong?
Seems test result is correct.
There are some gap between TRM and test result, need to…
Part Number: MSPM0L1227-Q1
Tool/software:
Hi Experts.
Regarding TRM of MSPM0 L-Series 32MHz Microcontrollers.
Both 0 and 1 mentioned enableed. Is 0 disable?
Best regards,
Ito
( 93d3848a-5635-4363-aaf2-23fdadfa3fb9)
Part Number: MSPM0L1227 Other Parts Discussed in Thread: SYSCONFIG Tool/software: Hi, I can select only 12 ADC ch in sysconfig (Software view).
Under "Reserved Peripheral" view I can see all ADC 21ch but here I can't generate the .c and .h files…