Hi Aiden,
GPIO0 may not have the resistor populated on the EVM, hence why it was not working.
Register 0x1A Status Register can provide more information on the connection. See section 3.8 from the technical reference manual.
Best Regards,
Aya Khedr
Part Number: AWR1443 Hi Experts,
Our customer are using EVM1000 to obtain raw-data of sensor AWR1443Boosster following the instructions from EVM technical manual, while it can not work, with errors: [13:26:37] Status: Failed, Error Type: RESP TIMEOUT [13…
Hi Allison Nguyen,
Thanks for your reply.
I moved to an example SCI echo back to check whether I was receiving characters from the terminal or not.
The very first error I see in the example is given below:
Remember. Here SW1 is on (For UART to USB connection…
Part Number: LP-AM243 Other Parts Discussed in Thread: SYSCONFIG Tool/software: Hello TI
We are testing CPSW ports using LP-AM243, we deleted one ethernet phy which was previous connectted to RGMII1 and replace it with our FPGA,RGMII1 tx channels are…
Part Number: UCC5870-Q1 Tool/software: Wanted to post an update to the related question but the thread was locked. We were able to fix the issue. In order to not trigger the VCE_CLP safety on startup, we had tied VCE_CLP to GND2, however we needed to…
Thank you for the prompt response!
I was able to read the range profile in the MSS and confirmed that it is transmitted via UART.
However, there is an issue. When I plotted the range profile received via UART, I was unable to obtain a graph with the shape…
Hello Arnab,
Unfortunately MSS Power Up async event was not received is an error that can be caused by several different issues, but the problem is due to connection issues between DCA1000 and computer with no relation to the mmWave sensor. I would attempt…
Part Number: AWR2243
Tool/software:
I followed the porting guide from mmWaveLink docs and managed to run mmWaveDFP on my FPGA. I am running mmWaveLink_SingleChip_NonOS_Example and using SPI communication.
MMWL_powerOnMaster and MMWL_firmwareDownload…
Hi David,
We apologize for not acquiring the relevant TI LaunchPad. The chip model we are currently utilizing is CC2674R106T0RGZ.
We conducted tests on other chip-based modules such as CC2674P10, CC1354R10, and CC1354P10 without encountering any issues…
Part Number: TMS320C6745 Tool/software: I need add UART driver code into a very old project which developed with DSP/BIOS v5.42.1.9.At first i used EDMA3 to transfer received data from Rx FIFO of UART1 to data buffer in SRAM,two problem appears,one was…