Part Number: NE5534A Other Parts Discussed in Thread: TLV9364 Hello,
We are seeing NE5534AD are Last buy process now and it is going to EOL announced by PDN# 20230522005.3
This OP-amp was employed on many of Audio application with a unique sound characteristics…
Part Number: NE5534A Other Parts Discussed in Thread: NE5534 , SA5534 , OPA134 The NE5534AP is listed as LTB.
There is a new part on the 5534 page: NE4434APE4.
But all links for this part appear to be broken.
Is this part available & is there…
Part Number: NE5532A Other Parts Discussed in Thread: NE5534A , OPA1677 , OPA134 Hello,
According to sales team's information, NE5532A/NE5534A include G4 and E4 devices are going to EOL caused by FAB matter.
Could you suggest us TI replacement device…
Part Number: SA5534A Other Parts Discussed in Thread: NE5534A , , NE5534 , SA5534 Hello,
I wanted to ask about the difference of the parts SA5534A and NE5534A. The only difference that I found when checking the datasheet was that the SA5534A is specified…
Part Number: NE5534A Other Parts Discussed in Thread: NE5534 Hi All,
We have a problem with DC offset in one of our products, related to the input bias current of the NE5534's that we're using. The issue wasn't present when the product was designed…
Part Number: TAD5242 Other Parts Discussed in Thread: OPA2891 , , NE5534A , OPA1632 , TPA3126D2 , PCM4104
The datasheet says the differential outputs can provide 2VRMS, which is 2.8Vp-p on each output pin. It also says that in line output mode it can…
Hi again Kai
The comparator inputs are at low mpedance; the non-inverting input is driven by an op-amp, actually an NE5534A, and NOT a TL081 as shown. Under quiescent conditions the signal here is a +/- 2V peak triangle.The inverting comparator input…
Hi Andrew,
keep in mind that the noise data of datasheet are only typicals which can widely vary from chip to chip.
Many years ago we had to screen all of our NE5534 for the use in a professional audio application. We had to hand select the NE5534…
Hi all,
the first two photos are from the link given by Michael. The last photo is from Kanji. The photos shall show the similarities:
Popcorn noise can even be seen in voltage regulators like the LM317. And I remember that we had to use the…