Part Number: TS321-Q1 Other Parts Discussed in Thread: OPA171-Q1 , , LM2904V Hi team,
Could you please kindly help to confirm if TS321-Q1 has similar spec as OPA171-Q1 which shows as below, if have, them could you please kindly help to share it to us…
Hi Siddharth,
The OPA171-Q1 device has a common mode voltage range from (V-) - 0.1V to (V+) - 2V over temperature. Please see below.
The OPA171 uses a complementary pair input stage so the input common mode voltage can go from the negative supply…
Part Number: TLV3701-EP Other Parts Discussed in Thread: TLV3701-Q1 , OPA171-Q1 , , TLV3701 , TLV3702 , TLV2464 , SN74LVC1G66-Q1 , TS5A3159 I use TLV3701-EP to convert open-gnd connection to 5V logic level. I have 4 of these comparator circuits on the…
Hi Che Wen,
Che Wen Yeh said: The differential input full-scale voltage will be approximately ±1.25 V, output range would be 0~5V
The proposed circuit violates the input and output linear operating requirements. 5Vdc single supply rail is unable to…
Part Number: OPA4171-Q1 Other Parts Discussed in Thread: OPA171 Tool/software: Hi team,
Could you share the input to output propagation delay time with me for OPA4171-Q1?
Thanks!
Ethan Wen
Part Number: OPA171 Other Parts Discussed in Thread: TLV171-Q1 Hello,
I have a design with fairly large closed-loop gain where I want to use OPA171.
Upon checking open loop gain specification I noticed figure 21 which seems weired to me (3 curves…
Other Parts Discussed in Thread: TPD4S009 , TCAN1042HG Hi,
I attach my PV ROOF CONTROLLER schematic,
and please check the peripheral settings of UCC2897.
the PWM is not operate normally at my end customer side.
It may something wrong, but I couldn…