Part Number: OPA188-Q1
Hi Experts,
Could you please share the Functional Safety FIT rate document (based on IEC 62380 / ISO 26262)?
And customer want the Mission Profile is on Motor Control of IEC 62380.
Thank you in advance.
Part Number: INA293 Other Parts Discussed in Thread: OPA188 , BUF634A , THS3491 Hi Team,
I want to design an electronic dc load. I drew a test board as in attachment. I have some concerns and questions about the design in schematic.
1. I plan to…
And, I think I finished scanning the TI product trees for post 2015 <50MHz Introductions - omg, this is quite impressive, lot of work here to fill in the parametric fields, but this is the list I came up with the slightly modified descriptions - this…
Part Number: OPA2180 Other Parts Discussed in Thread: OPA2377 , OPA2376 , OPA2188 , , OPA2325 , OPA2397 , OPA2392 , OPA2387 , OPA2182 , OPA2187 , OPA180 , OPA188 Hi experts,
Q1. Could you please tell me your recommended devices that is alternative…
Part Number: UCC28951-Q1 Other Parts Discussed in Thread: OPA188 , UCC28951 , TL431 I am using UCC28951-Q1 in CC/CV mode. I am using external OPA188 based Error Amplifier while Internal error amplifier (EA) is used as unity gain by shorting EA- with COMP…
Hi Tomas,
This is Stewart .
Long time no communication.
Our customers have another big problem with using the OPA188.
They can replacment from LM201AN(On-SEMI) to OPA188. OPA188 is not working the aging test(1weeks).
Q1. Pls checkt to the…
Part Number: OPA211 Other Parts Discussed in Thread: OPA188 Hi team,
I want to get the error voltage for the op amp. For exmple, OPA211, Vos is 20uV, Ib is 50nA,CMRR is 120dB.
Q1: If Ib causes an error voltage Vib and CMRR causes an error voltage…
Thanks, Garrett.
Garrett Satterfield said: 5us settling time
Q0. Is settling time equal to Sample/update rate (MSPS)?
Garrett Satterfield said: DAC60504 - 12-bit, 4ch, 5us settling time, QFN
I think this will be perfect, except for the packaging…
Mark,
You apparently have a full-scale voltage on the shunt R11 of about 25mV, or so. I'm a bit concerned about the influence of offset voltage. Your original selection had a max offset voltage of 2.5mV, a 10% error relative to full scale. Can you tolerate…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…