Hello Art Kay,
I would like to clarify the output-drive capability and stability of the OPA192-Q1 for my application.
If I use a single-ended 7.5 V supply for the OPA192-Q1, can it reliably generate a 6 V output while driving a maximum load current…
Part Number: OPA192-Q1 Other Parts Discussed in Thread: OPA192 I have a precision 5 V reference available at the IN+ input, and I need to generate an adjustable output range of 0 V to 1.5 V from this reference.
I would like to achieve this with very…
Part Number: OPA192-Q1 Other Parts Discussed in Thread: OPA192 Hi team,
My customer want to transfer "slope of pulse" as shown in attached material, but it doesn't work as expected.
Could you check attached material and support it?
Best regards…
Part Number: OPA192-Q1 Hello OPAMP team,
I'm Gilberto.
I have two questions.
1. which is the Overvoltage protection value when the power is off?.
2.which is the Input Impedance value when the power is off?
Thanks,
Gilberto DIAZ
Part Number: OPA192-Q1 Other Parts Discussed in Thread: OPA192 Hello OPAMP team,
I'm Yuta Kurimoto TIJ FAE.
I got some questions from our customer. Could you give answer?
Q. When the VCM get close to V+, why Vos, EN, en, CMRR get worse? I'd like…
HI David,
The most similar device to the OPA191 (2.5-MHz) in automotive grade is the OPA2192-Q1 (10-MHz). The OPAx192-Q1 is a 36-V Precision, Rail-to-Rail Input/Output, Low-Offset Voltage, Low-Input Bias Current Op Amp With e-trim . The OPAx192-Q1 offset…
Part Number: TLE2037A-Q1 Other Parts Discussed in Thread: TLV197-Q1 , OPA197-Q1 , OPA192-Q1 , TLE2141-Q1 , OPA1612-Q1 Hello,
Good day, Customer wants a TLE2037a-Q1 pin to pin device within 1Mhz. Could you please give a recommandation. Thank you.
Part Number: ADS7887 Other Parts Discussed in Thread: OPA377-Q1 , OPA192-Q1 , TLV197-Q1 , OPA376-Q1 , OPA320-Q1 , OPA197-Q1 , OPA340 , OPA340-EP Hello,
I am trying to determine how closely the qualification test data matches with AEC-Q100 level screening…
The linear output swing of any op amp is a condition used in AOL test and is a function of output current (Iout).
Thus, in the case of OPA192-Q1 the max/min linear output swing over -40C to 125C temperature is 300mV from either rail with 10k load (Iout…
Hi Raj,
The OPA192 products are in stock. If you are looking for specific package, it may be out of stock current, see the information and link below. OPA192-Q1 is the automotive version of OPA192 part.
https://www.ti.com/product/OPA192?utm_source…