Part Number: OPA196 Tool/software: Hi Team,
We are using the OPA196IDBVR in our design and need clarification regarding its input offset voltage drift.
According to the datasheet, the typical value is specified as <0.5 μV / ⁰C at VS=±18V, VCM=(V+…
Part Number: OPA196 Other Parts Discussed in Thread: OPA4317 , OPA317 I can't get the Spice Models for OPA196 and OPA4317 from the website, Where I can get it?
Part Number: OPA196 Other Parts Discussed in Thread: OPA197 , OPA228 , TINA-TI , OPA202 Dear Technical Support Team,
Are OPA196 and OPA197 unity gain stable?
Datasheets described unity gain bandwidth.
Do you have selection guide for unity gain stable…
Part Number: OPA196 The OPA196 datasheet lists the input bias current maximum at 20pA. Does this 20pA maximum apply over the entire common mode input voltage ranges as depicted in figure 4 ?
It's difficult to interpret what the Ib vs. CM voltage variation…
Other Parts Discussed in Thread: OPA196 I need to simulate a circuit using an OPA196. It does not show up in the PSpice part Search pane. I looked in the C:\Cadence\PSpiceTI\PSpiceTI\Lib\library.zip file and it is present there. How can I get access to…
Part Number: OPA196 ABS1.TSC
Hi, TI.
I am currently designing an absolute value circuit while looking at JAJA204. However, if the input voltage is negative, the output voltage will not drop to 0V. How can I reduce it to 0V?
Sincerely.
Yuzur…
Part Number: OPA196 Hello together,
can I suplly the OPA196 with a normal 9 V Battery, or I have to consider anything?
Do I have to restrict the supply current general?
Thanks for helb,
Marvin
Part Number: OPA196 Other Parts Discussed in Thread: ALP Hello, I designed a circuit that takes the output of a hall and amplified that output using the op amp given in the description. However I am finding that the output voltage is lower than what I…
Part Number: OPA196 Other Parts Discussed in Thread: OPA197 Hi team,
OPA196 seems to be seen some distortion in the following condition.
Evaluation in voltage follower - Positive supply = +24V - Negative supply = -5V - Input signal frequency = 500kHz…
Part Number: OPA196 Other Parts Discussed in Thread: OPA1656 Hi Team,
My customer is just looking for amps specified Min and Max for "Input voltage noise density"(Especially Min value).
Min values (or Variation Data) are needed to pick up the device…