Part Number: OPA211-HT Other Parts Discussed in Thread: OPA211 Hi,
In the attached file, why the IB and Vos of the 2nd op amp of OPA211 is not considered in the calculations ? Thanks Doc50.docx
Part Number: OPA211 Other Parts Discussed in Thread: LMH13000 Tool/software: Hi,
I want to design a constant current source composed of an operational amplifier and a push-pull circuit (for example, as shown in the following figure). May I ask if there…
Part Number: OPA211-HT Other Parts Discussed in Thread: OPA2333-HT , OPA211 Hi,
During testing Vos and IB for my newly purchased op amps (OPA211-HT & OPA2333-hT), I observed that my measurments were way above the datasheet parameter values. I discussed…
Part Number: OPA211 www.ti.com/.../slyt343 shows
Figure 6. A 50-kHz, differential-input, single-ended-output, second-order 0.5-dB Chebyshev low-pass filter (AV = +10 V/V)
Where C2 is a single capacitor across the inputs rather than two capacitors…
Part Number: OPA211-HT Other Parts Discussed in Thread: OPA211 , OPA2333 Hi,
I am purchsing QTY=2 unit of OPA211SHKJ and QTY=2 of OPA2333SHKJ to perform a verification test on these units (OMG, they are expensive!) . I was trying topurchase an EVM proto…
Part Number: OPA211-HT Other Parts Discussed in Thread: OPA2333-HT , , OPA211 , OPA2333 Hi,
Unlike the datsheet of OPA2333-HT, the datasheet of OPA211SHKJ does not show characteristics in extreme hot temperature, i.e. 210C. Almost all charateristics…
Part Number: OPA211 Hello
I ordered part # OPA211AIDR and from what i see on the data sheet the part marking should be OPA 211 A but the parts we received are marked
A TI OPA
211 K
42CFED
How do we know if we have the correct parts since they…
Part Number: OPA211-HT Other Parts Discussed in Thread: TINA-TI , Tool/software: Hello,
I need a .lib file of this component for a TINA-Ti simulation.
It could be another operational amplifier that can works at 200ºC.
Thanks in advanced.
Asie…
Part Number: OPA211 Dear Sirs
I need to connect for layout reason the Pin_1 with the Pin_2 of the OpAmo OPA211. On the datasheet I read "No internal connection. This pin can be left floating or connected to any voltage between (V–) and (V+)". It seems…
Part Number: OPA211 Tool/software: "I attempted to import TINAOPAx211.lib and perform a DC analysis with temperature variation in TINA. However, an error occurred during the process. Details are as follows:
TINA Version: 9.3.150.328 SF-TI
Operating…