Part Number: OPA2170 Other Parts Discussed in Thread: LM7705 , OPA2990 Hi Team,
My Japanese customer has a question about OPA2170AIDCU. The question is below:
This op amp is used as a voltage follower for the buffer before and after the voltage dividing…
Part Number: OPA2170 Hi All , can anyone please let me know when does the internal clamp diode start conducting 10ma? as per datasheet the inputs should not exceed vcc by more than 0.5v so does this apply o the input pins after the internal 2.5K resistor…
Part Number: OPA2170 Other Parts Discussed in Thread: TINA-TI Hi,
Please tell me the characteristics of OPA2170AIDR.
Question: Please let me know if you know the minimum and maximum values of Open-loop output resistance Ro. Operating conditions are…
Part Number: OPA2170 Hello,
The OPA2170 datasheet shows a DSG / WSON package.
I don't see it as an orderable package on TI.com. Is this package option available?
If so, should the thermal pad be connected to Ground? Or could it be left floating…
Other Parts Discussed in Thread: OPA2170 , OPA170 I'm using an OPA2170 in an unusual circuit. The part is configured as an instrumentation amp with a gain of 10, and most of the time, it is operated linearly... the inputs never exceed the supply rails…
Other Parts Discussed in Thread: OPA2170 , OPA192 , OPA130 , OPA172 , OPA137 I'm observing that the OPA2170 has Input Differential Over-Voltage Protection Diodes. I do not see these mentioned in the datasheet anywhere.
Can someone confirm this?
I…
I also need the power the package can dissipate. (For derating exercise.) I do not see this in your data sheet. Can you tell me what it is for each dual package of the opa2170?
Part Number: LM2766 Other Parts Discussed in Thread: OPA2170 , , TLV2402 Hello!
I am using LM2766 with 3.3V input and 6.6V output. It only powers a dual amplifier, OPA2170 (about 250 uA total current).
LM2766 has an enable signal, which should be…