Part Number: OPA2320 Other Parts Discussed in Thread: ADS127L11 , , OPA2206 , PGA280 Hello TI,
I'm working on a signal chain that inputs into an ADS127L11 for measurement. The chain was designed and simulated specifically for low noise.
Unfortunately…
Part Number: BUF634A Other Parts Discussed in Thread: OPA2206
Hi Team,
Good day!
I am posting this in behalf of the customer.
I'm using a BUF634AIDDAR to buffer a 1MHZ 50% square wave (from 0V to 10V). The output of the buffers seems…
Part Number: TLV9001 Other Parts Discussed in Thread: OPA2206 , OPA2310 Hello team,
Does signal input without power supply give damage to TLV9001?
(3V DC is input to input pin without power supply. The buffer configuration will be used for monitoring…
Part Number: TL074 Other Parts Discussed in Thread: , OPA2206 , OPA206 , OPA2310 , TLV9154 Hi team,
Could inverting/ no-inverting input be high impedance when VCC not powered? Thanks.
Hi Mitchell,
Mitchell Gresham said: then limit the input which could be up to +-30V to the +-20V on the rails.
Per your description, this is my interpretation. Please see if it is correct. There is no feedback between one op amp from others. It looks…
Part Number: OPA2205 Other Parts Discussed in Thread: OPA2206 Hi team,
To confirm, for Figure 6-22 at the datasheet, the caption describes voltage noise density but the y-axis shows current noise density. Also, the Figure 6-22 looks the same with Figure…
Hi Kazuya,
Kazuya Nakai59 said: Q. Is it allow to apply any voltage to IN+/IN- pin when LM324B is in power down (no power applied) if the voltage is less than 40V?
For LM324B, the input has the same voltage threshold, which is less than 300mV when…
Hi Henry,
Below a couple of ideas:
The INA592 difference amplifier configured on G=2 has a differential input impedance of 6kΩ + 6kΩ = 12kΩ. Since the sense resistor is 1kΩ and relatively large compared to the 12kΩ input impedance of the instrumentation…
Hello Yumiko,
What is the magnitude of voltage that you expect at the input to the amplifier? The inputs should not exceed the positive and negative supplies for the OPA656. There are no parts with internal over-voltage protection at the bandwidth range…
Other Parts Discussed in Thread: OPA2206 , THP210 , OPA2182 , OPA2387 , OPA197 , OPA391 , INA821 , INA826 , LPV821 , OPA369 PRAMPS in lab and field instrumentation
Analytical lab equipment can be used for early detection of diseases and drug development…