Part Number: TLV9062 Other Parts Discussed in Thread: TLV9002 , TLV9042 , TLV9052 , , ADC101S021 , OPA2322 , OPA2320 Hello team,
Could you please provide the output voltage swing (Vo) value for larger RL such as RL>1MOhms?
I'd appreciate if you provide…
Amey,
You could try by implementing a single-ended to differential circuit with a couple opamps. Based on the max voltage rail (3.3V) you might want to look into RRIO amplifiers, so you can use the most of your mic dynamic range as possible. OPA family…
Nakagawa,
Sample test results for more amplifier enable responses are below.
LMV982MM Clean response other than a 0.1V to 0.2V dip at end of enable time.
OPA2363 Clean response on this sample
OPA2322 Clipped high and low during the enable time…
Hi Nesh,
Does the customer need 24V supply? If they do, I would start by looking at the OPA2172 or the TLV2172. Those devices will be pretty close and can support the higher supply voltage.
Otherwise, the OPA2322 might also be worth a look.
If…
Hi Bill,
I think OPA2320 and OPA2322 fit most of your requirements and have 0.50mm pitch SON packages.
I've used the Selguide to narrow down the search:
Regards,
Hooman
Hello Lorenzo,
I have been looking for a TLV2475 replacement that will provide the high output current drive and the shutdown capability for each channel. One possible option is the OPA2322S; a dual. It provides higher performance overall than the TLV2475…
Part Number: OPA2365-Q1 Other Parts Discussed in Thread: OPA2365 , OPA2322-Q1 Hello,
I have a client who uses OPA2365 and ADS795X to test Voltage sample.
Customers want to replace OPA2365 with cheap ones.
I'd like to ask if OPA2322-Q1 can be used…
Farhan,
GBP of 1MHz is nowhere sufficient to obtain 80kHz usable bandwidth in a close loop gain of 100 but GBP of 80MHz is probably an overkill. OPA360 has a fixed internal gain of 2 so you may not use it for your desired gain of 100. Most of our amplifiers…